On the Calculation of FlexCAN Mailbox region

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

On the Calculation of FlexCAN Mailbox region

跳至解决方案
744 次查看
JihongZhang
Contributor II

Hi,

I am writing a FlexCAN driver. Refer to S32K144 FlexCAN driver. The MB area calculation function and data manual description do not match. Is there any mistake in my understanding?

As described in the data manual, the MB interval of 8 payloads is 16 bytes, but 32 bytes are calculated in the code. Is there any problem in understanding?

source Code:

volatile uint32_t* FLEXCAN_GetMsgBuffRegion(
CAN_Type * base,
uint32_t msgBuffIdx)
{
#if FEATURE_CAN_HAS_FD
uint8_t payload_size = FLEXCAN_GetPayloadSize(base);
#else
uint8_t payload_size = 8U;
#endif

uint8_t arbitration_field_size = 8U;
uint32_t ramBlockSize = 512U;
uint32_t ramBlockOffset;

uint8_t mb_size = (uint8_t)(payload_size + arbitration_field_size);
uint8_t maxMbNum = (uint8_t)(ramBlockSize / mb_size);

ramBlockOffset = 128U * (msgBuffIdx / (uint32_t)maxMbNum);

/* Multiply the MB index by the MB size (in words) */
uint32_t mb_index = ramBlockOffset + ((msgBuffIdx % (uint32_t)maxMbNum) * ((uint32_t)mb_size >> 2U));

return &(base->RAMn[mb_index]);
}

 

JihongZhang_0-1670381572362.png

 

0 项奖励
回复
1 解答
727 次查看
Senlent
NXP TechSupport
NXP TechSupport

I didn't understand the logic of your formula, I did a simple calculation based on this function

for example:

msgBuffIdx 0 1 2 3
RAMn[CAN_RAMn_COUNT] RAMn[0] RAMn[4] RAMn[8] RAMn[12]

 

The offset address of RAMn is 0x80,the size of each RAMn[x]  is 4 bytes and each offset is 4 bytes, and the space occupied by one MB is exactly 16 bytes. Is there any problem?

在原帖中查看解决方案

0 项奖励
回复
4 回复数
735 次查看
Senlent
NXP TechSupport
NXP TechSupport

I didn't get your point, isn't MB_SIZE equal to 16 here?(payloadSize =

Senlent_0-1670400058234.png

 

0 项奖励
回复
732 次查看
JihongZhang
Contributor II

My understanding is that this function is used to calculate the starting address of MB, but why is this function used to calculate the second MB of an 8-byte load offset by 32 bytes? Shouldn't it be 16 bytes? (1/32)*512 + (1%32)* 16 = 8 dword, 0x80 + 0x20 = 0xa0. But isn't the interval between two MB in the MB structure description 16 bytes?

JihongZhang_0-1670400672568.png

 

0 项奖励
回复
728 次查看
Senlent
NXP TechSupport
NXP TechSupport

I didn't understand the logic of your formula, I did a simple calculation based on this function

for example:

msgBuffIdx 0 1 2 3
RAMn[CAN_RAMn_COUNT] RAMn[0] RAMn[4] RAMn[8] RAMn[12]

 

The offset address of RAMn is 0x80,the size of each RAMn[x]  is 4 bytes and each offset is 4 bytes, and the space occupied by one MB is exactly 16 bytes. Is there any problem?

0 项奖励
回复
693 次查看
JihongZhang
Contributor II

hi Senlent,

As shown in the figure below,What is written in the document is the same as what you described, but why is the calculated result of this function different from what is described in the document? The calculated address of Mb [0] is 0x80, while Mb [1] is offset by 32 bytes.

JihongZhang_0-1670407139260.png

 

 

0 项奖励
回复