Hi,
I am using S32R247RM Board. I would like to implement CSE on Board.
But i found CSE peripheral is disabled, when i looked in trace.
I have gone through AN4234 and AN5418 Application Notes and i understood the Commands.
but when i tried to implement it, no CSE related command is executing on board.
I tried by giving CSE_INIT(0x15) command but this is also not running.
Do i need to add something in Lauterbach file to enable and run CSE commands?
please suggest me something that i can do to enable CSE.
Thank you.