LPSPI Chip Select Pins on S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI Chip Select Pins on S32K144

1,744 Views
ewest
Contributor I

Is it possible to use GPIO pins as chip select for SPI and leave the chip select pins PCS[3:0] available for other functions? From what I have read in the documentation it seems like the programmer is required to use the specified chip select pins.

0 Kudos
Reply
3 Replies

1,407 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, it is possible to use GPIO as a chip select and toggle it manually when needed. But if you use SDK, be aware that the SPI drivers do not support this customization. If don't use the drivers, there should be no problem.

Regards,

Lukas

0 Kudos
Reply

1,407 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

I agree with you, but I think I should add this detail: if the LPSPI is used in slave mode the is mandatory to use PCS pins.

Best regards,

Razvan

0 Kudos
Reply

1,407 Views
yashwanth411
Contributor II

Hi Erin,

You can use normal GPIO pin as chip select. I tested like that it is working fine. You select any PCS[0:3] pin and configured that pin to GPIO. Which PCS pin you are selecting, write that value in PCS field in TCR register in LPSPI.

Regards,

Yashwanth

0 Kudos
Reply