Hello,
This is the first time to power up the S32K144_EVB using FreeMASTER.
My computer connects well with the S32K144_EVB but an issue comes up when I tried to process the "4.2 FreeMASTER JumpStart project download" shown in the following link.
https://www.nxp.com/document/guide/get-started-with-the-s32k144evb:NGS-S32K144EVB
When I tried section 4.2 in the above link, the following error popup comes up.
"Could not open project file from link: http://www.nxp.com/assets/downloads/data/en/application-software/S32K144EVB_OOBE.pmpx"
For your reference, I attached a capture of the warning popup in this thread.
Any help will be appreciated. Thank you very much.
已解决! 转到解答。
I could be able to solve the issue by downloading a file from the following link and importing the file using FreeMASTER.
https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true
I could be able to solve the issue by downloading a file from the following link and importing the file using FreeMASTER.
https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true
Hi jungx148,
Sorry for the inconvenience we bring you!
You can download the S32K144_EVB_JumpStart_Firmware.zip
attached in: Cannot Connect to S32K144 (Neither FreeMaster nor S32DS)
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------