Installation of latest SW32K1 LIN stack version 1.0.2 CD01 on S32DS v3.5 fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installation of latest SW32K1 LIN stack version 1.0.2 CD01 on S32DS v3.5 fails

Jump to solution
418 Views
M_SCH
Contributor III

Hello,

I have recently migrated to S32DS v3.5 and tried to integrate th e latest version of RTD, FreeRTOS and Linstack that is provided by NXP. I have attached a text file that covers the output provided under Help --> Installation Details in S32DS.

The issue is that I try to install SW32K1 LIN stack version 1.0.2 CD01 but the installation is done just partially as in ticket. The installation window displays

M_SCH_0-1717670353618.png

and after un-checking all ticks from the boxes the error message is displayed

Cannot complete the install because one or more required items could not be found.
Software being installed: LINSTACK S32K1 1.0.2.202209300724 (com.nxp.LINSTACK.S32K1.root.1.0.2.feature.feature.group 1.0.2.202209300724)
Missing requirement: LINSTACK S32K1 1.0.2.202209300724 (com.nxp.LINSTACK.S32K1.root.1.0.2.feature.feature.group 1.0.2.202209300724) requires 'org.eclipse.equinox.p2.iu; com.nxp.RTD.S32K1XX.1.9.0.feature.feature.group 0.0.0' but it could not be found

Does this mean, that this version of the Linstack is not compatible with the RTD version S32K1_S32M24X Real Time Drivers AUTOSAR R21-11 Version 2.0.0 P04 that is available online?

Apparently version com.nxp.RTD.S32K1XX.1.9.0.feature.feature.group 0.0.0 is required but your download page offers not such version.

M_SCH_2-1717672482705.png

 

Can you point out either how to fix this issue or which versions of

  • RTD
  • FreeRTOS
  • Linstack 

can be used with S32DS v3.5 together?

Note, that the Linstack version 1.0.1 is also installed but 

M_SCH_0-1717673468033.png

is still missing as shown in the image above.

If you require more information let me know.

 

Best regards

 

M_SCH

0 Kudos
Reply
1 Solution
396 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @M_SCH 

The SW32K1 SW32M24X LIN Stack version 1.0.2 with RTM qualification is already available and can be downloaded through S32K1 Reference Software > Automotive SW - S32K1_S32M24X - LIN Stacks > SW32K1 SW32M24X LIN Stack version 1.0.2. 

This software version is compatible with the S32K1_S32M24X Real-Time Drivers ASR 4.4 & R21-11 Version 2.0.0 and S32 Design Studio for S32 Platform 3.5.

 

B.R.

VaneB

View solution in original post

1 Reply
397 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @M_SCH 

The SW32K1 SW32M24X LIN Stack version 1.0.2 with RTM qualification is already available and can be downloaded through S32K1 Reference Software > Automotive SW - S32K1_S32M24X - LIN Stacks > SW32K1 SW32M24X LIN Stack version 1.0.2. 

This software version is compatible with the S32K1_S32M24X Real-Time Drivers ASR 4.4 & R21-11 Version 2.0.0 and S32 Design Studio for S32 Platform 3.5.

 

B.R.

VaneB