Installation of S32DS for S32 platform with S32 RTD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installation of S32DS for S32 platform with S32 RTD

Jump to solution
663 Views
john24
Contributor III

Hello,

I would like to install S32DS for S32 platform, with S32 RTD, for software development targeting S32K344. I went to S32 RTD page and downloaded HVBMS package:

john24_0-1712610709314.png

The downloaded file is 'NXP_Multi_Installer_08.04.24.095916_setup.exe'. However, when installing it, I got the following errors and eventually have to quit the installation process:

 

john24_2-1712610819603.pngjohn24_3-1712610986838.pngjohn24_4-1712611025857.png

Please advise on how to resolve such "SSL certificate problem...". Thank you.

 

Tags (2)
0 Kudos
Reply
1 Solution
535 Views
john24
Contributor III

Hi Robin,

I have this doc instead:

john24_0-1713288029778.png

By following the steps in the doc, I am able to install the sw tools and build the projects referenced in Ch. 5 of the document.

Thanks.

View solution in original post

5 Replies
617 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for replying to you so late. There was a problem with the company's network a few days ago. I just saw your question on the internal system today.

I tried to download BMS Application 0.8.0 today. I haven't encountered the problem you mentioned. Does your colleague's computer have the same problem downloading? Have you contacted your IT to check on the issue?

Best Regards,
Robin

0 Kudos
Reply
614 Views
john24
Contributor III

Hi Robin,

Thank you for the reply. After working with our IT team and disabled our firewall temporarily, I was able to run 'NXP_Multi_Installer_09.04.24.125506_setup.exe', which then eventually downloaded all 16 components:

john24_0-1712940584677.png

However, now my question is: What is the correct order of going into each of the above 16 folders and install the component properly? Our plan is to develop RTD based application software, with FreeRTOS, targeting the S32K344 MCU, and have it running on the RD-K344BMU eval board initially. If successful, then we will attempt to run such software on our own custom board with the S32K344 MCU on-board.

Please advise. Thanks.

0 Kudos
Reply
547 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Have you downloaded the Ug763620 - HVBMS Software Installation Guide (2.0) Please note that this document is confidential and therefore can only be downloaded with a valid NDA through the link I sent you via private message.

0 Kudos
Reply
536 Views
john24
Contributor III

Hi Robin,

I have this doc instead:

john24_0-1713288029778.png

By following the steps in the doc, I am able to install the sw tools and build the projects referenced in Ch. 5 of the document.

Thanks.

542 Views
john24
Contributor III

Hi Robin,

I searched for "Ug763620 - HVBMS Software Installation Guide (2.0)" while logged in at the NXP site, but cannot find such document. Could you please provide it?

Thank you.

 

John

0 Kudos
Reply