Implementing LPIT DMA SPI for UJA1169TK/F in S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementing LPIT DMA SPI for UJA1169TK/F in S32K144

Jump to solution
1,348 Views
KARTHKSARODE
Contributor III

Hi 

I was implementing the SPI functionality with the help of DMA , I found an useful example from daniel

Detailed description says :

  • LPIT_ch0 triggers DMA_ch0 periodically (1ms)
  • Every trigger starts a minor DMA loop (8 bytes) transfer to the LPSPI1 TX FIFO
  • There are 8 minor loops per one major loop (64 bytes in 8ms)
  • LPSPI1 sends two 32bit frames every 1ms
  • LPSPI1 RX data are masked, they are not stored in the RX FIFO

Then I modified , it to :

  • LPIT_ch0 triggers DMA_ch0 periodically (1ms)
  • Every trigger starts a minor DMA loop (2 bytes) transfer to the LPSPI1 TX FIFO
  • There are 3 minor loops per one major loop 
  • LPSPI1 RX data are masked, they are not stored in the RX FIFO
  • DMA source array is uint16_t lpspi_tx_data[3]={0xFD00,0x0B00,0x0700};
  • Each time a successful transmission of word , RDR register will be having 0xFDEF,0x0B08,0x0700 respectively  
  • In current configuration DMA is taking care of tx FIFO , I'm reading the received register by myself (Once interrupt is generated for Transfer word complete , I can see the value in RDR register)
  • This configuration is working perfectly fine

Later I tried to add one more DMA channel to read RDR register value:

  • Added LPIT_ch1 to trigger DMA_ch1 periodically(1ms)
  • Every trigger starts a minor DMA loop (2 bytes) transfer to the receive array from RDR register 
  • There are 3 minor loops per one major loop 
  • So basically for every 1ms DMA will read RDR register 
  • From my observation , I'm guessing the issue is with delay of LPIT (I guess I'm reading RDR register at wrong time)
  • Right now , I don't have any scope to verify the timing , please help to solve this issue
  • Let me know what might be the issue 

Let me know if some more clarification is required from my side 

I have attached the project from the reference 

Best Regards
KARTHIK SV
Tags (4)
0 Kudos
Reply
1 Solution
1,334 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @KARTHKSARODE,

For the RX channel, there is no need for a periodic trigger.

You can use the normal mode (17.2.3 Modes of operation) and disable the triggerring in DMAMUX_CHCFG.

The minor loop transfer is then triggered by the LPSPI_SR[RDF] flag only.

Which is configurable.by LPSPI_FCR[RXWATER].

 

Regards,

Daniel

View solution in original post

1 Reply
1,335 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @KARTHKSARODE,

For the RX channel, there is no need for a periodic trigger.

You can use the normal mode (17.2.3 Modes of operation) and disable the triggerring in DMAMUX_CHCFG.

The minor loop transfer is then triggered by the LPSPI_SR[RDF] flag only.

Which is configurable.by LPSPI_FCR[RXWATER].

 

Regards,

Daniel