I need an example:S32k344 reads and writes SD card through SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I need an example:S32k344 reads and writes SD card through SPI

ソリューションへジャンプ
667件の閲覧回数
SCoder41
Contributor I

Do NXP official have examples of reading and writing SD cards?


笔记

SD.png

0 件の賞賛
返信
1 解決策
567件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @SCoder41 

To make sure the FlexIO as SPI works properly, please try testing the SPI example with the settings you require.

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
640件の閲覧回数
SCoder41
Contributor I

Can I use Flexio_SPI to read and write SD cards on s32k344?

0 件の賞賛
返信
615件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @SCoder41,

It is possible if the FlexIO module supports the SD card's operating requirements. Unfortunately, we do not provide any examples for this application. The functionality is on your implementation.

0 件の賞賛
返信
605件の閲覧回数
SCoder41
Contributor I

I can not receive data from sd card,but The oscilloscope shows that the SD card has responded.My array has no data,that’s why?

1.jpg2.jpg3.png4.png5.png6.png7.png8.png

9.png

0 件の賞賛
返信
568件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @SCoder41 

To make sure the FlexIO as SPI works properly, please try testing the SPI example with the settings you require.

0 件の賞賛
返信
505件の閲覧回数
SCoder41
Contributor I

Thanks,my DMA configuration is incorrect.

0 件の賞賛
返信
650件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @SCoder41 

I am afraid, that we do not provide any examples for SD Cards through SPI.

It is important to mention that certain commands are not available for the SPI mode of interfacing and also, the speed will be lower than the SD mode. But this kind of interfacing is simpler especially since most microcontrollers have built-in SPI hardware modules. For S32K3 devices the module that provides the interface between the host system and the SD card is the Ultra Secured Digital Host Controller (uSDHC), which is only present in S32K328, S32K338, S32K348, and S32K358 devices.

 

B.R.

VaneB

0 件の賞賛
返信
639件の閲覧回数
SCoder41
Contributor I

Can I use Flexio_SPI to read and write SD cards on s32k344?

0 件の賞賛
返信