How to wake wake up MFS2633 from LPOFF Mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to wake wake up MFS2633 from LPOFF Mode?

跳至解决方案
480 次查看
shiqi_seventeen
Contributor III

hello everyone ,

How to wake wake up MFS2633 from LPOFF Mode?

Please give me some Detailed Process

Thanks!

0 项奖励
回复
1 解答
454 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

The LPOFF mode is intended to place the system in a fully OFF state with no system supplies active. The logic circuitry is supplied internally allowing proper wake up from any of the available wake-up mechanisms, with the minimum current consumption possible.

To enter LPOFF mode, some conditions and commands are required. You can send a SPI request to go to LPOFF mode from INIT_FS state or Normal mode. Two commands must be sent, the second command
(transition to LPOFF mode) must be sent within 10ms after the first command (transition to Pre-LPOFF mode) is sent. Passed the 10ms, the FS26 will go to the INIT_FS state.

Write the below commands to FS_LP_REQ register:
1. FS_LP_REQ[7:0] = A5h ➙ Transition to Pre-LPOFF mode
2. FS_LP_REQ[7:0] = 5Ah ➙ Transition to LPOFF mode

Before sending the request, you must select a way to wake-up from low power or else, the FS26 will be
stuck until a power-on reset event. The wake up signals must be enabled through the M_WIO_CFG register: 

Capture.JPG

The picture below illustrates the transition to the LPOFF mode.

Capture 1.JPG

BR, Tomas

在原帖中查看解决方案

0 项奖励
回复
2 回复数
455 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

The LPOFF mode is intended to place the system in a fully OFF state with no system supplies active. The logic circuitry is supplied internally allowing proper wake up from any of the available wake-up mechanisms, with the minimum current consumption possible.

To enter LPOFF mode, some conditions and commands are required. You can send a SPI request to go to LPOFF mode from INIT_FS state or Normal mode. Two commands must be sent, the second command
(transition to LPOFF mode) must be sent within 10ms after the first command (transition to Pre-LPOFF mode) is sent. Passed the 10ms, the FS26 will go to the INIT_FS state.

Write the below commands to FS_LP_REQ register:
1. FS_LP_REQ[7:0] = A5h ➙ Transition to Pre-LPOFF mode
2. FS_LP_REQ[7:0] = 5Ah ➙ Transition to LPOFF mode

Before sending the request, you must select a way to wake-up from low power or else, the FS26 will be
stuck until a power-on reset event. The wake up signals must be enabled through the M_WIO_CFG register: 

Capture.JPG

The picture below illustrates the transition to the LPOFF mode.

Capture 1.JPG

BR, Tomas

0 项奖励
回复
444 次查看
shiqi_seventeen
Contributor III
Wow,Cool!Thanks Tomas
And there is also a question:When MC33772C is sleeping, IO cannot be maintained at the level before MC33772C sleeps.And how to make it maintained at the level before sleeps?
0 项奖励
回复