Hi.
I have to use SPI 3 channels and I am using EB TRESOS.
- SPI 1 channel is activated well.(communicate with TLE9262)
- I have to add SPI 2 channels as master
I think that I have to add SPI physical unit as below.
But when I added SPI physical unit, MCU did not work at Trace32
- build was done.
- If I removed SPI physical unit, MCU worked.
How can I add 2 more SPI channel?
Hi Kim JungHyun,
I have tried to use your configuration to create a simple project and I can see it run normally.
I also create one more channel and add it to the SpiJob_0. I also can see it work normally.
Please find the project in the attached file.
Best regard,
Hung
Hi Kim JungHyun,
Could you please share your MCAL package version and SPI, MCU configuration for us to check it first.
Best regards,
Hung.
HiKim JungHyun,
Could you please send the configuration in .epc file. It will easy for us to check/modify your configuration with the .epc file.
Best regards,
Hung.