I just started with AUTOSAR and I have S32K144EVB I want to find instructions on how to use Tresos to generate config file and put it in S32DS for debug, build... Can anyone tell exactly where I should start from where?
Generation of a new project from an existing project file. Construction 3. Debugging is the fifth. A final destination. 9 ... Our IDE and development environment, Eclipse, will begin to load. This will then... Go to File > New >S32DS Application Project... Navigate to (1) C/C++ Build, (2) Settings, and (3) Target Processor in the build's configuration.
Creating a project from existing project file. 3. Building. 5. Debugging. 6. Terminal. 9 ... It will begin to load the eclipse environment and IDE we will be using to write and test code. It will then ... File > New >S32DS Application Project ... In the build settings, go to (1) C/C++ Build, (2) Settings, (3) Target Processor