How to determine the reset cause between external pin reset and internal reset on the S32K?
During the internal reset, the reset pin was set to low for about 500 us.
In the case of an external pin reset, how long should the reset pin be set to low?
Hi Ken3,
Each reset source has an associated field in the Reset Control Module (RCM) System Reset Status (RCM_SRS) register.
You can check the vaule of RCM_SRS.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------