How to configure the MPU to protect RAM sections in S32K344

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure the MPU to protect RAM sections in S32K344

895件の閲覧回数
lega_06
Contributor I

Hi.

I've been trying to configure the MPU to protect RAM sections, I mean I want to change the RAM section to Read-only, but I couldn't set it, I have these sections in MPU.

    /*Ram unified section */
    rbar[6]=0x20400000UL;
    rasr[6]=0x160B0023UL;

    /*Ram non-cache section plus */
    rbar[7]=0x20420000UL;
    rasr[7]=0x030C001FUL;

    /*Ram stack section*/
    rbar[8]=0x20424000UL;
    rasr[8]=0x130B001FUL;

    /*Ram shareable section*/
    rbar[9]=0x2043C000UL;
    rasr[9]=0x130C0029UL;

within my linker file,I have the same address like in each rbar

int_sram_c0 : ORIGIN = 0x20400000, LENGTH = 0x00020000 /* 98kB */ /*128kB*/
int_sram_no_cacheable_c0 : ORIGIN = 0x20420000, LENGTH = 0x00004000 /* 16kB */

int_sram_stack_c0 : ORIGIN = 0x20424000, LENGTH = 0x00004000 /* 64kB */ /*16kB*/
int_sram_c1 : ORIGIN = 0x20428000, LENGTH = 0x00004000 /* 16kB */
int_sram_no_cacheable_c1 : ORIGIN = 0x2042C000, LENGTH = 0x00004000 /* 16kB */
int_sram_stack_c1 : ORIGIN = 0x20430000, LENGTH = 0x00008000 /* 32kB */
int_sram_shareable : ORIGIN = 0x2043C000, LENGTH = 0x00004000 /* 16kB */
ram_rsvd2 : ORIGIN = 0x20440000, LENGTH = 0 /* End of SRAM */

I've tried to set Read-only, within RAM unified section the AP encondig according to the next table 

lega_06_0-1690397757293.png


But I can still write in that RAM area , I would expect to see a some reset in my board after writting in this area , also somehow the only RAM section that I can put in Read only is Ram shareable section within region#9 , if change from rasr[9]=0x130C0029UL to rasr[9]=0x160C0029UL.I'm not sure why this is happening.

How should I configure RAM unified as Read-only ? , is there anything else that I need to set it up? 

 

0 件の賞賛
返信
5 返答(返信)

858件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@lega_06

Senlent_0-1690435965467.png

0x130C0029UL->AP[2:0] = 011 = RW->Full accsss

0x160C0029UL->AP[2:0] = 110 = RO->Read only,by privileged or unprivileged software.

0 件の賞賛
返信

851件の閲覧回数
lega_06
Contributor I

Hi, @Senlent  I have set those bits for Read only in Region#6 (RAM unified section), but I can write into this section, because after setting the MPU, I try to write  4 bytes with 0xFF in 0x20400000, and I can see it from 0x20400000 until 0x20400004, although I have that region set as Read only I can still write it.

I wonder why I can still write in this section that should be protected.

0 件の賞賛
返信

788件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@lega_06

Senlent_0-1690517178035.png

I tried to configure it according to your method, and the program entered hardfault.
Can you provide a complete project file, I need to reproduce the problem, which takes a lot of time.

0 件の賞賛
返信

729件の閲覧回数
lega_06
Contributor I

I can't put all project, but I found in Tressos that we have 0 RAM Sector in our project, I'm wondering if we need to set these 4 RAM sections within Tressos as well?

0 件の賞賛
返信

712件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@lega_06

Thank you for your reply,
I don't know the EB tool you are using, and I don't know the process of configuring MPU on EB, so I can't give you a suitable suggestion,
You can create a new topic and add EB or MCAL as the keyword. We will have experts in EB and MCAL to help you answer your questions.
I'm sorry for not being able to provide a valid opinion.

0 件の賞賛
返信