I am currently using the TCM feature of S32K3x in my RTD.
S32DS: 3.5
RTD: S32K3_RTD_3_0_0_D2303_ASR_REL_4_7_REV_0000_20230331
Best regards,
Chris
解決済! 解決策の投稿を見る。
Hi @Chris-Sun
The PRTN2_COFB1_CLKEN[REQ62] field for Cortex-M7_0 is enabled at reset as you can see from the image below:
B.R.
VaneB
Hi @Chris-Sun
The PRTN2_COFB1_CLKEN[REQ62] field for Cortex-M7_0 is enabled at reset as you can see from the image below:
B.R.
VaneB
Hi @VaneB
Thank you for your response to my post.
Best regards,
Chris
Hi Mr.Sun:
------
From your appeal description, I cannot infer a solution to the problem. At present, K312 does not seem to support the enable configuration of TCM-CM7_0_CLK. Can you provide a more detailed solution.
The problem I am currently facing is that after the interrupt is enabled and triggered, I cannot enter the interrupt. I don't know if it is related to TCM-CM7_0_CLK not being enabled?