How MR-CANHUBK344 setup CAN parameters

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How MR-CANHUBK344 setup CAN parameters

跳至解决方案
389 次查看
huaixi_wei
NXP Employee
NXP Employee

Hello Expert,

https://www.nxp.com/design/design-center/development-boards-and-designs/automotive-development-platf...

My customer is investigating MR-CANHUBK344. Can customer setup CAN parameters such as baud rate/sampling position/ID filter, etc by IEEE1722 ACF protocol? That is to say the link partner setup the CAN parameters by IEEE1722 ACF protocol.

0 项奖励
回复
1 解答
350 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

probably it would be possible, if ACF message will contain such data and user will implement/parse that.
A given MR_CANHUBK3_IEEE 1722 demo example just convert an IEEE 1722 ACF-CAN fame and send it over FlexCAN (and vice-versa). No setting of baud rate/ID filter, etc is implemented upon ACF message reception. FlexCAN init is done at application start and does not change.

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
2 回复数
351 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

probably it would be possible, if ACF message will contain such data and user will implement/parse that.
A given MR_CANHUBK3_IEEE 1722 demo example just convert an IEEE 1722 ACF-CAN fame and send it over FlexCAN (and vice-versa). No setting of baud rate/ID filter, etc is implemented upon ACF message reception. FlexCAN init is done at application start and does not change.

BR, Petr

0 项奖励
回复
310 次查看
huaixi_wei
NXP Employee
NXP Employee

Hi @PetrS ,

Thanks for your quick reply! It is helpful.

0 项奖励
回复