Hello, dear. I am using s32k144 board for motor control. I want use a 12 V adapter. What must be the ampere of the adapter that do not damage the board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hello, dear. I am using s32k144 board for motor control. I want use a 12 V adapter. What must be the ampere of the adapter that do not damage the board?

960 次查看
mahdikazemi12
Contributor I

Hello, dear. I am using s32k144 board for motor control. I want use a 12 V adapter. What must be the ampere of the adapter that do not damage the board?

1 回复

896 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if we are talking about these development kits:

S32K144 3-phase PMSM Development Kit|NXP 

S32K144 3-phase BLDC Development Kit|NXP 

... then power supply is included in the package and the parameters are 12V and 5A.

Regards,

Lukas