Hard fault during hse firmware install

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hard fault during hse firmware install

1,177 Views
vikmonti7804
Contributor III

Hi,

    We flashed the hse firmware in the mcu and also We are initializing the MCU clock in our bootloader firmware. after reset the mcu I am experiencing the hard fault in MCU clock init from register level.

Then i commented the MCU clock init in bootloader firmware and then program is running without any hardfault.

Does it mean HSE is initializing the clock inside its firmware?

Or what can be reason for the hard fault, any clue?

please provide answers.

Tags (1)
0 Kudos
Reply
7 Replies

1,146 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please check if it is related to the reasons mentioned in the following discussion:
If I don't give s32k312 delay, the CAN stop during operation
S32K3_HSE_BUG_RTD2.0.x


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,127 Views
vikmonti7804
Contributor III

Hi robin,

        You can try with the board with HSE firmware installed on it and use the example code Dio_Example_S32K312, then you will see that the firmware is going into hard fault due to the function called Mcu_InitClock(McuClockSettingConfig_0);.

If i comment this function from the main file then there is no hard fault and led start toggling so my question.

How is this LED toggling without clock init?

Does HSE firmware is initializing the clock for MCU?

Please let me know these answers.

 

0 Kudos
Reply

1,122 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Could you share the S32DS version you are using and also the RTD version? So that I am able to verify if this is a problem related to a specific version of the tool.

Also, have you checked the two discussions mentioned in my last reply?

0 Kudos
Reply

1,116 Views
vikmonti7804
Contributor III

I am using RTD version is 4 4 0 and SW Version 2 0 3

DS version i am using Version: 3 4

I tried 

Changes done in file structure Mcu_aClockConfigPB_VS_0 in the file Clock_Ip_VS_0_PBcfg.c.

Change the value from 1 to 0 for FIRC clock and DIO example code is starts to run with HSE firmware.

But i need to justify why this is happening?

what is the reason behind this ?

Please check attached image.

0 Kudos
Reply

1,108 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

After the HSE FW is installed, the highest 3 bits(APP_CORE_ACC) of the GPR register are set to 0, which means that the application core cannot change the FIRC divider.

36.5.13 Configuration REG_GPR (CONFIG_REG_GPR) APP_CORE_ACC.png

However, the RTD 2.0.x code does not check if it can be changed, so the system will directly enter the hard fault.

In HSE-RM, it says the FIRC divider can be modified by call the HSE service.

Robin_Shen_0-1715326895261.png

Robin_Shen_1-1715326895421.png

0 Kudos
Reply

1,103 Views
vikmonti7804
Contributor III

So how much is the clock frequency for core from HSE?

Does HSE FW initialize the clock ? and at what frequency?

Do we need to initialize clock additionally in application?

Please clear asap.

0 Kudos
Reply

1,083 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

The proper operation of the HSE subsystem depends on the correct configuration of the clocks CORE_CLK, HSE_CLK, AIPS_SLOW_CLK, AIPS_PLAT_CLK, etc. Therefore, users need to follow the chapter 14.2.2.2 Clock Frequency Options for Devices of RM758223-HSE-B Firmware Reference Manual - V2.3(2.3).pdf, otherwise the HSE may not operate properly, or even HSE FW will be erased. Please initialize clock in your application.

0 Kudos
Reply