Hello,
I want to utilize one of the GPIO pin as digital output ( as they can be configured as temperature sensors and as digital input or output)
So in order to make GPIO1 as digital output; I wrote 12 to the register BCC_REG_GPIO_CFG1_ADDR
and in order to make it high, I wrote 2 to BCC_REG_GPIO_CFG2_ADDR
I did check the status of the pins using BCC_REG_GPIO_STS_ADDR register and got the value 202 indicating GPIO 1 is high.
But in hardware; I have taken a wire from the conjunction point of C74 AND R40 , yet I'm not getting any voltage there.
Kindly suggest a solution.
Thank you
I got it sorted, GND had to be w.r.t to MC33771B, got it !!