Freertos debug issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freertos debug issue

Jump to solution
2,769 Views
AchrafOukheir
Contributor III

Hi everyone,

I'm facing an issue while debugging a simple FreeRTOS project and I would appreciate some assistance. I am working with sk32k344 (HVBMS) and using the s32ds IDE. For debugging, I am using the PEmicro Debugger: Multilink Universal Rev C.

 

The problem I'm encountering is that I have four tasks in my project, but I am unable to set breakpoints and debug the code. Additionally, it seems that FreeRTOS is not being detected properly.

 

AchrafOukheir_0-1712238313135.png

I would like to know if there are any specific configurations or settings that I need to apply in order to enable debugging and ensure that FreeRTOS is recognized correctly.

Thank you in advance for your help!

 

the  Example is :

AchrafOukheir_1-1712238549135.png

 



Tags (4)
0 Kudos
Reply
1 Solution
2,747 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @AchrafOukheir 

I will be helping you in the thread Breakpoint FreeRtos debugging.

 

B.R.

VaneB

View solution in original post

0 Kudos
Reply
2 Replies
2,747 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @AchrafOukheir 

I will be helping you in the thread Breakpoint FreeRtos debugging.

 

B.R.

VaneB

0 Kudos
Reply
2,736 Views
AchrafOukheir
Contributor III

Thank you. If the breakpoints are resolved, the FreeRTOS debugging features will work.

0 Kudos
Reply