For the first time or a virgin S32K3, can I call Hse_Ip_ServiceRequest to install HSE firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

For the first time or a virgin S32K3, can I call Hse_Ip_ServiceRequest to install HSE firmware

320 次查看
CarlOfVmax
Contributor II

For the first time or a virgin S32K3, can I call Hse_Ip_ServiceRequest to install HSE firmware?

标记 (1)
0 项奖励
1 回复

292 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

No. The HSE firmware is not installed on a virgin S32K3, so HSE Service is not available. 
If you have installed HSE_DEMOAPP_S32K3XX_0_2_1_0.exe, you will find the answer in NXP HSE BASIC FW FAQ.pdf (C:\NXP\HSE_DEMOAPP_S32K3XX_0_2_1_0\demo_security_installer\docs\NXP HSE BASIC FW FAQ.pdf) 
Q: How do I install HSE FW on a virgin device without secure boot?

How do I install HSE FW on a virgin device without secure boot NXP HSE BASIC FW FAQ.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励