Hello,
I am trying to test the functionality of the FlexCAN peripheral on the NXP S32K3X4EVB-Q172. The NXP provided-example (FlexCAN_Ip_Example_S32K344) is configured in loop-back only mode, but I would like to test actually sending messages over the CAN bus.
I've tried out the various example projects posted on this thread: https://community.nxp.com/t5/S32K/FlexCAN-IP-example-not-running-in-normal-mode-on-S32K344-EVB/m-p/1... but each of the projects trigger a bus shut off (i.e. BOFFDONEINT = 1b). I did notice that that thread was in reference to an NXP TJA1153 transceiver, whereas the transceiver on my board appears to be an NXP TJA1043 (not sure if this makes a major difference).
Anyway, stepping through the driver code (in debug mode) in the FlexCAN_Ip_SendBlocking() function reveals that FlexCAN_StartSendData() runs successfully (it returns FLEXCAN_STATUS_SUCCESS), but the transmission always timesout in the following while-loop which waits for transmission (i.e. timeElapsed >= mS2Ticks).
Is there perhaps something obvious I'm missing? Like a jumper that needs to be configured or some other hardware pre-condition? I've tried testing by hooking up CANH_OUT (as well as CAN0_TX) to an oscilloscope, as well as using CANoe, but nothing appears on either.
I've attached all my version info in case it's relevant (see ver_info.txt), as well as a snapshot of the contents of the FlexCAN 0 peripheral registers (see can_reg_snap.txt).
Solved! Go to Solution.
Thank you!
This example does indeed work, both under an oscilloscope and under CANoe.
Hi
The CAN PHY on S32K3X4EVB-Q172 is TJA1043, but it is TJA1153 on S32K3X4EVB-Q257 and S32K3X4EVBQ257ND. Due to CAN PHY differences, you cannot directly use the various example projects posted on that thread.
Best Regards,
Robin