FS26 RTD - FS0B pin release at start-up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS26 RTD - FS0B pin release at start-up

ソリューションへジャンプ
1,105件の閲覧回数
pagdav
Contributor III

Dear all,

in the function Sbc_fs26_ExitDebugMode()defined in the file .\RTD\src\CDD_Sbc_fs26.c (S32K3XX FS26 AUTOSAR R21-11 Version 3.0.0), the function Sbc_fs26_ReleaseSequence() is called even if the device is not in Debug Mode. Since the call to the function Sbc_fs26_ExitDebugMode() cannot be excluded from execution, I get the FS0B pin released at the end of start-up.

Thank you for your support.

@pagdav

0 件の賞賛
返信
1 解決策
797件の閲覧回数
pagdav
Contributor III

I opened a ticket to NXP support and I received the response. The recognized issue has been resolved in the FS26 RTD driver version FS26 SBC AUTOSAR R21-11 Version 4.0.0 CD01.

元の投稿で解決策を見る

0 件の賞賛
返信
13 返答(返信)
1,069件の閲覧回数
pagdav
Contributor III

Hi @guoweisun,

I would like to not release the FS0B pin at start-up (NORMAL mode), but using the RTD drivers I always get FS0B released. This is due to the Sbc_fs26_ExitDebugMode() function which cannot be excluded from execution in the function Sbc_fs26_NormalFSSequence().

Thanks for your support.

0 件の賞賛
返信
1,067件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Before enter into normal mode you have to release FS0B/FS1B.

0 件の賞賛
返信
1,064件の閲覧回数
pagdav
Contributor III

I would like to not enter automatically in NORMAL MODE at start-up. I need to enter in NORMAL mode when I receive i CAN message, using the function Sbc_fs26_ReleaseSequence() to release both pins.

0 件の賞賛
返信
1,061件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

 Could you please let me know which status the SBC in before receive CAN message?

 

 

0 件の賞賛
返信
1,058件の閲覧回数
pagdav
Contributor III

The SBC should be in the status "Safety Outputs asserted" (Figure 14 - Simplified functional state diagram).

0 件の賞賛
返信
1,056件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Seems in that state can't enter normal mode by CAN message

guoweisun_0-1717746053266.png

 

0 件の賞賛
返信
1,052件の閲覧回数
pagdav
Contributor III

Dear @guoweisun,

my request is:

I would like to switch manually from "Safety Outputs asserted" state to "Fail-Safe normal state" state using the function Sbc_fs26_ReleaseSequence().

In the actual RTD driver, the switch from "Safety Outputs asserted" state to "Fail-Safe normal state" state is automatic at the end of start-up.

Functions call sequence:

Sbc_fs26_InitDevice() -> Sbc_fs26_NormalFSSequence() -> Sbc_fs26_ExitDebugMode() -> Sbc_fs26_ReleaseSequence()

0 件の賞賛
返信
924件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You should refer to below flow chart whatever manually or automatically enter into normal mode from the Safety Outputs asserted state.

guoweisun_0-1718116020478.png

 

0 件の賞賛
返信
920件の閲覧回数
pagdav
Contributor III

I can't do it manually because it is done automatically by the function Sbc_fs26_InitDevice().

Please, check the code of the function Sbc_fs26_InitDevice() before to answer.

0 件の賞賛
返信
914件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Unfortunately I can't code to you about manual step to release FSXB then enter into normal mode,what I can do for you is provide the flow chart ,you have to do it by yourself,if don't fully understand the steps please let me know.

0 件の賞賛
返信
912件の閲覧回数
pagdav
Contributor III

The function Sbc_fs26_InitDevice() is implemented in the RTD driver, auto-generated by NXP S32DS. I can't modify the RTD driver.

0 件の賞賛
返信
798件の閲覧回数
pagdav
Contributor III

I opened a ticket to NXP support and I received the response. The recognized issue has been resolved in the FS26 RTD driver version FS26 SBC AUTOSAR R21-11 Version 4.0.0 CD01.

0 件の賞賛
返信
1,073件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

If I understand your questions correctly, you don't need enter into debug mode and exist into debug mode.

You can see below flow chart of SBC,if you don't use emulation mode,you can skip this and after release RSTB directly enter into INIT mode.

guoweisun_1-1717740619485.png

 

 

0 件の賞賛
返信