External clock signal levels

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External clock signal levels

378件の閲覧回数
JensFleischhacker
NXP Employee
NXP Employee

I'm confused about the S32K1 datasheet and the 2 statements about the external clock

For low detection you need to be below 1.15V, for high above 0.7*VDD but on the other hand a Vexp_pp value of more than 0.8V is sufficient.

What kind of external clock signal levels are supported ? I have a 1.25V square wave signal is that suffiecent or do I need a VDD related signal ?

For S32K3 there are no levels define in the datasheet. Is that possible at all and if yes how should the signal look like. Same as for S32K1 ?

0 件の賞賛
返信
1 返信

362件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Certainly it is expected square wave of level VDD for high and VSS for low. Do not compare it with internal oscillator, it is different mode.

Grey zone between VILmax and VIHmin is just transitory area (with included hysteresis).

In S32K3, requirements are the same that the digital/logic levels (VIL/VIH), it is just not specified separately.

0 件の賞賛
返信