External clock signal levels

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

External clock signal levels

325 次查看
JensFleischhacker
NXP Employee
NXP Employee

I'm confused about the S32K1 datasheet and the 2 statements about the external clock

For low detection you need to be below 1.15V, for high above 0.7*VDD but on the other hand a Vexp_pp value of more than 0.8V is sufficient.

What kind of external clock signal levels are supported ? I have a 1.25V square wave signal is that suffiecent or do I need a VDD related signal ?

For S32K3 there are no levels define in the datasheet. Is that possible at all and if yes how should the signal look like. Same as for S32K1 ?

0 项奖励
1 回复

309 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Certainly it is expected square wave of level VDD for high and VSS for low. Do not compare it with internal oscillator, it is different mode.

Grey zone between VILmax and VIHmin is just transitory area (with included hysteresis).

In S32K3, requirements are the same that the digital/logic levels (VIL/VIH), it is just not specified separately.

0 项奖励