Enabling a PWM chanel in S32k146

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling a PWM chanel in S32k146

428 Views
akhilranga
Contributor IV

Hi there,

Can someone please assist me with the enabling a PWM outpit channel for sending a very specific signal as output .

Signal that need to be sent is in the following format

akhilranga_0-1712819221175.png

for transmitting Data 0 : 1ms high level + 3ms low level

for transmitting Data 1 : 3ms high level + 1ms low level

 I want to send the 0x5555 which in Binary is 0101010101010101. So, i belive this can be send through the PWM output. If,yes. How can i set up the PWM for an output GPIO. And send the above mentioned signal

P.s: I am using a S32k14x EAR SDK v0.8.6

So, please kindly assist me in any way possible

0 Kudos
3 Replies

404 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

signal looks very similar as one mentioned in https://mcuoneclipse.com/2016/05/22/nxp-flexio-generator-for-the-ws2812b-led-stripe-protocol/ maybe you can refer to this or other links mentioned there.

BR, Petr

0 Kudos

395 Views
Salomi
Contributor I

Hi @PetrS ,

Currently i am trying to interface the LED Stripe WS2812B with  NXP S32k344 . I want to generate the PWM (24bits) to control the RGB LED . Please suggest which SW driver(Flexio_PWM , EMIOS_PWM ) should i need to use it for PWM generation. Please share me the configuration for the respective driver along with the any sample code if possible.

Thanks!

0 Kudos

275 Views
akhilranga
Contributor IV

Hi @PetrS 

I have tried to develop the code with out the requirement of PWM. But i am getting some system and syntax error from the software. which i couldn't able to resolve . attaching the code and the error information below. Please help me understand the error and also can you please judge my code. let me know anywhere i can improve or make changes. 

/* Including needed modules to compile this module/procedure */
#include "S32K146.h"
#include "Cpu.h"
#include "clockMan1.h"
#include "pin_mux.h"

volatile int exit_code = 0;
/* User includes (#include below this line is not maintained by Processor Expert) */
#include <stdint.h>
#include <stdbool.h>

//#define LED_PORT 	 PORTD
//#define GPIO_PORT	 PTD
//#define PCC_CLOCK	 PCC_PORTD_CLOCK
//#define LED1		 15U
//#define LED2		 16U

  #define LOCK_COMM  7 //Output


#define Lock_Status   1  //Locked: 1, Unlocked 0


#define LOCK_COMMAND   	 0xAAAA //1010 1010 1010 1010
#define UNLOCK_COMMAND 	 0x5555 //0101 0101 0101 0101



void delay_ms(uint32_t milliseconds)
{
    /* Delay function - do nothing for a number of cycles */
    uint32_t ticks = milliseconds*(SystemCoreClock / 1000);
    while(ticks--){}
}



void sendData( int dataLevel )
{


	if (dataLevel == 1)
	{
		// Data 1:
		// Turn on the LED
		PTE->PCOR |= (1 << LOCK_COMM);
        	delay_ms(3);

		// Turn off the LED
		PTE->PSOR |= (1 << LOCK_COMM);
        	delay_ms(1); // Total 4ms delay
	}
	else if (dataLevel == 0)
	{

		// Data 0:
        	// Turn on the LED
		PTE->PCOR |= (1 << LOCK_COMM);
        	delay_ms(1);

        	// Turn off the LED
		PTE->PSOR |= (1 << LOCK_COMM);
        	delay_ms(3); // Total 4ms delay
}
//void initOneWirePin(void)
//{
//    //configure GPIO pin PTE7 for command transmission
//    PTE->PDDR &= ~COMMAND_PIN_MASK; // Set pin as input (pull-up)
//}




int main(void)

{

  /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
  #ifdef PEX_RTOS_INIT
    PEX_RTOS_INIT();                 /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */
  #endif
  /*** End of Processor Expert internal initialization.                    ***/

    //initOneWirePin();

    // Enable clock to PORT E (where the LOCK_COMM is connected)
        PCC->PCCn[PCC_PORTE_INDEX] |= PCC_PCCn_CGC_MASK;

        // Set pin as GPIO
        PORTE->PCR[LOCK_COMM] |= PORT_PCR_MUX(1);


        // Set pin as output
        PTE->PDDR |= (1 << LOCK_COMM);




  while (1)
  {
	  int k = 0;
	  	if (Lock_Status == 1){
	  		// send 0xAAAA
	  		delay_ms(5); //sync. head

	  		for (int i = 0; i < 15; i++) {
	  			//sendData(1);
	  			//sendData(0);
	  			sendData((LOCK_COMMAND >> i) & 0x01); // Send each bit of the lock command 1 or 0
	  		}
	  		
	  		delay_ms(4); //ACK
	  	}
	  	else if(Lock_Status == 0){
	  		// send 0x5555
	  		delay_ms(5); //sync. head

	  		for (int i = 0; i < 15; i++) {
	  			//sendData(0);
	  			//sendData(1);
	  			sendData((UNLOCK_COMMAND >> i) & 0x01); // Send each bit of the unlock command 1 or 0

	  		}
	  		delay_ms(4); //ACK
	  	}
	  	delay_ms(200);
	  	if( k += 10)
	  	{
	  	break;
	  	}


  }

  /*** Don't write any code pass this line, or it will be deleted during code generation. ***/
  /*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/
  #ifdef PEX_RTOS_START
    PEX_RTOS_START();                  /* Startup of the selected RTOS. Macro is defined by the RTOS component. */
  #endif
  /*** End of RTOS startup code.  ***/
  /*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/
  for(;;) {
    if(exit_code != 0) {
      break;
    }
  }
  return exit_code;
  /*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/
}/*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/

/* END main */
/*!
** @}
*/
/*
** ###################################################################
**
**     This file was created by Processor Expert 10.1 [05.21]
**     for the Freescale S32K series of microcontrollers.
**
** ###################################################################
*/

 

 

In the below image you can also notice the error symbol in the project tree at sendData function. So, is there any issue with my sendData function.?

Screenshot (248).png

0 Kudos