Hi,
I try to test the action of ERM when i read different address of SRAM and peripheral RAM with EIM enabled.
but it seems that ECC signal-bit correct event occurred after EIM init directly without read SRAM
how can i trigger ECC signal-bit correct event after read specific RAM address instead of after enable EIM?
program in the pic is ERM example of sdk3.0.0.
Solved! Go to Solution.
Hi @Momiji,
The EIM is enabled within the EIM_DRV_Init() function.
If the error is injected to SRAM_U, the error is detected when it leaves the function and the core accesses the Stack.
You would need to read an SRAM_U address within the function.
Regards,
Daniel
Hi @Momiji,
The EIM is enabled within the EIM_DRV_Init() function.
If the error is injected to SRAM_U, the error is detected when it leaves the function and the core accesses the Stack.
You would need to read an SRAM_U address within the function.
Regards,
Daniel