Doze mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
653件の閲覧回数
QJ_HAPPY
Contributor I

If LPI2C can run in low power consumption (such as stop mode) (Doze mode is turned on), how can I know that LPI2C runs in stop mode? The program should stop at the position where it enters STOP?

0 件の賞賛
返信
1 解決策
643件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @QJ_HAPPY,

In the RM rev.14 (Table 39-4 Module operation in available power modes), you can see that LPI2C is fully-functional in STOP2, and it supports Async operations in STOP1 and VLPS.

danielmartynek_0-1669109844166.png

Fully-functional means that LPI2C can send the commands in the TX FIFO and receive data.

Table 52-10 & Table 52-11 list wakeup interrupts.

 

BR, Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
644件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @QJ_HAPPY,

In the RM rev.14 (Table 39-4 Module operation in available power modes), you can see that LPI2C is fully-functional in STOP2, and it supports Async operations in STOP1 and VLPS.

danielmartynek_0-1669109844166.png

Fully-functional means that LPI2C can send the commands in the TX FIFO and receive data.

Table 52-10 & Table 52-11 list wakeup interrupts.

 

BR, Daniel

0 件の賞賛
返信
632件の閲覧回数
QJ_HAPPY
Contributor I

Thanks for your reply

0 件の賞賛
返信