Disable and re-enable UART with VLPS mode of operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disable and re-enable UART with VLPS mode of operation

ソリューションへジャンプ
1,538件の閲覧回数
__invited__hari
Contributor V

Hello Team,

This is about S32K148 power down modes and LPUART.

I am able to switch between VLPS and RUN modes with UART enabled.

But my use case is to enable UART only during RUN mode and disable that communication in VLPS mode. 

I am able to disable the interrupt, but not renabled with below code sequence

PSEUDO CODE:

INT_SYS_DisableIRQ ( LPUART2_RxTx_IRQn );
POWER_SYS_SetMode ( VLPS, POWER_MANAGER_POLICY_AGREEMENT )
INT_SYS_EnableIRQ ( LPUART2_RxTx_IRQn );

Can someone suggest with any example code to do the same please?

Thanks,

Hari

ラベル(1)
タグ(2)
1 解決策
1,291件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

The INT_SYS_DisabledIRQ and INT_SYS_EnableIRQ functions disable and enable the interrupts in the NVIC registers only. The LPUART module is off in stop modes if LPUART_CTRL[DOZEEN] = 1 anyway.

The FIRC, SPLL, SOSC clock sources must be disabled before the transition to VLPS and the current SDK driver disables them. So, if you want to use LPUART once it is in RUN again, you need to ensure that the LPUART clock is enabled.

Regards,

Daniel

元の投稿で解決策を見る

3 返答(返信)
1,291件の閲覧回数
__invited__hari
Contributor V

I just found a solution, but not sure that is the right way of doing it.

What I did is, I switched the clock source of LPUART to FIRC and configured that clock as disabled in 'low power' mode.

Please confirm that this is the correct solution to my use case as explained above.

0 件の賞賛
返信
1,292件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

The INT_SYS_DisabledIRQ and INT_SYS_EnableIRQ functions disable and enable the interrupts in the NVIC registers only. The LPUART module is off in stop modes if LPUART_CTRL[DOZEEN] = 1 anyway.

The FIRC, SPLL, SOSC clock sources must be disabled before the transition to VLPS and the current SDK driver disables them. So, if you want to use LPUART once it is in RUN again, you need to ensure that the LPUART clock is enabled.

Regards,

Daniel

1,291件の閲覧回数
__invited__hari
Contributor V

Thanks Daniel for the clarification

0 件の賞賛
返信