Difference between module clock and CHI clock in FlexCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between module clock and CHI clock in FlexCAN

758件の閲覧回数
KKumar
Contributor II

Hi NXP,

i am bit confuse between the module clock and CHI clock of FlexCAN module (as shown in image)of S32K.

Plz explain the difference and their uses.

KKumar_0-1648561780409.png

 

 

0 件の賞賛
返信
1 返信

746件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@KKumar

below infos comes from S32K-RM Chapter 55.2.1 Overview

Senlent_0-1648605507919.png

The Protocol Engine (PE) submodule manages the serial communication on the CAN

bus:

  • Requesting RAM access for receiving and transmitting message frames
  • Validating received messages
  • Performing error handling
  • Detecting CAN FD messages

The Controller Host Interface (CHI) submodule manages message buffer selection for

reception and transmission, taking care of arbitration and ID matching algorithms for

both CAN FD and non-CAN FD message formats.

The Bus Interface Unit (BIU) submodule controls access to and from the internal

interface bus, in order to establish connection to the CPU and to other blocks. Clocks,

address and data buses, interrupt outputs, DMA and test signals are accessed through the

BIU.

BR!

      Jim,

 

0 件の賞賛
返信