Hi @Omkar9903
It is not possible to control the timing of the DMA ISR by simply setting a parameter. However, you can generate a periodic DMA trigger event using the PIT or when a transmit buffer becomes empty or a receive buffer becomes full, periodically. Refer to section 13.4.2.1 (Enable a source with periodic triggering) of the S32K39 and S32K37 Reference Manual, Rev. 3.
Could you provide more details on the implementation you are looking for?
BR, VaneB
Hi @Omkar9903
It is not possible to control the timing of the DMA ISR by simply setting a parameter. However, you can generate a periodic DMA trigger event using the PIT or when a transmit buffer becomes empty or a receive buffer becomes full, periodically. Refer to section 13.4.2.1 (Enable a source with periodic triggering) of the S32K39 and S32K37 Reference Manual, Rev. 3.
Could you provide more details on the implementation you are looking for?
BR, VaneB