DMA configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DMA configuration

145 次查看
Omkar9903
Contributor I

Hi,

I am using s32k96 UC & configured of dmaLogicChannel_Type_0 with CH16 using DMA_IP_HW_INST_1 interrupt.

I have attached the one image I want to change the ISR time but not getting which parameter is configure for ISR time.

BR Omkar.

0 项奖励
回复
1 回复

84 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Omkar9903 

It is not possible to control the timing of the DMA ISR by simply setting a parameter. However, you can generate a periodic DMA trigger event using the PIT or when a transmit buffer becomes empty or a receive buffer becomes full, periodically. Refer to section 13.4.2.1 (Enable a source with periodic triggering) of the S32K39 and S32K37 Reference Manual, Rev. 3.

Could you provide more details on the implementation you are looking for?

 

BR, VaneB

0 项奖励
回复