Could not connect to target

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could not connect to target

3,369件の閲覧回数
lohrsistemas
Contributor IV

I'm try to program the device PS32K144UFVLL0N47, but, the following error occurred:

Could not connect to target.
Please check power, connection and settings.SEGGER J-Link GDB Server V6.14a Command Line Version

JLinkARM.dll V6.14a (DLL compiled Feb 27 2017 18:41:26)

-----GDB Server start settings-----
GDBInit file:                  none
GDB Server Listening port:     2331
SWO raw output listening port: 2332
Terminal I/O port:             2333
Accept remote connection:      localhost only
Generate logfile:              off
Verify download:               on
Init regs on start:            on
Silent mode:                   off
Single run mode:               on
Target connection timeout:     0 ms
------J-Link related settings------
J-Link Host interface:         USB
J-Link script:                 none
J-Link settings file:          none
------Target related settings------
Target device:                 S32K144
Target interface:              JTAG
Target interface speed:        auto
Target endian:                 little

Connecting to J-Link...
J-Link is connected.
Firmware: J-Link PRO / Flasher PRO V4 compiled Jan 27 2017 17:07:01
Hardware: V4.00
S/N: 694200245
Feature(s): JFlash, GDB
Checking target voltage...
Target voltage: 4.89 V
Listening on TCP/IP port 2331
Connecting to target...ERROR: Could not connect to target.
Target connection failed. GDBServer will be closed...Restoring target state and closing J-Link connection...
Shutting down...

Any idea?

Thanks

0 件の賞賛
返信
3 返答(返信)

2,372件の閲覧回数
lohrsistemas
Contributor IV

I checked the reset pin and measured 1.250V. Is it correct? 

0 件の賞賛
返信

2,372件の閲覧回数
lohrsistemas
Contributor IV

If I try to use OpenSDA instead of Jlink, the following error occurs:

pastedImage_1.png

This is strange because when I use the 0N77P version, everything works, but with 0N47, I cant.  

I would very much like an answer as I have customers requesting my product. I have already sent prototypes to 0N77P version, which I have no more.

0 件の賞賛
返信

2,372件の閲覧回数
lohrsistemas
Contributor IV

I put the PS32K144UFVLL0N47 on the EVB FRDMPK144-Q100, but even so I was not able to write / debug. Is 0N47 hardware different from 0N77?

0 件の賞賛
返信