Compatiability of MemAcc module for Fee from BSW stack suppliers - S32K358, S32K388

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Compatiability of MemAcc module for Fee from BSW stack suppliers - S32K358, S32K388

跳至解决方案
1,012 次查看
manuprasad_v
Contributor I

Hello,

I am using the following components from the RTD delivery for configuring NvM stack with NXP data flash.

Mem_43_INFLS

MemAcc

We can see that the Fee Cluster of NXP will be referring to MemAcc module, Don't see a similar configuration in the ETAS Fee module.

I would like to know whether this stack can be configured using ETAS Fee module. Also, please let us know the mandatory modules that need to be used to configure data flash in NXP RTD delivery (Mem_43_INFLS, MemAcc, Fee for the stack?)

 

Thanks,

Manuprasad

0 项奖励
回复
1 解答
957 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Could you explain what is ETAS Fee module?
Fee is module avaiable from version Autosar 4.4 and previous, and it is replaced by MemAcc module in version R21-11 and afterward
THe mandatory modules need to use MemAcc is mentioned in IM (Integration Manual) document of MemAcc module in installed package:

cuongnguyenphu_0-1700810362049.png

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
917 次查看
manuprasad_v
Contributor I

Hello,

I think the FEE module is not replaced, the FLS module is replaced with MEM_43_INFLS and MemAcc. We have received the FEE module in the RTD delivery from NXP. (SW32K388_RTD_4.4_R21-11_4.0.0_CD01).

manuprasad_v_0-1701789920580.png

 

ETAS is a third-party software vendor that supplies BSW modules for our use case Fee.

Thanks,

Manuprasad

0 项奖励
回复
913 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
Sorry, it's my mistake.
Yes you're correct that Fee is not replaced.
Fee module from NXP is follow AUTOSAR Fee driver software specification Autosar ver R21-11.
We also have some deviations from the requirement and it mentioned in FEE User Manual's document, which is include in FEE module in the package install.
Please check this User Manual, section Deviations from Requirements to see detail which requirement that we excluded and compare with ETAS FEE
For the compatibility with ETAS Fee, we haven't have experience with ETAS Fee so I'm not sure about this point

0 项奖励
回复
958 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Could you explain what is ETAS Fee module?
Fee is module avaiable from version Autosar 4.4 and previous, and it is replaced by MemAcc module in version R21-11 and afterward
THe mandatory modules need to use MemAcc is mentioned in IM (Integration Manual) document of MemAcc module in installed package:

cuongnguyenphu_0-1700810362049.png

 

0 项奖励
回复