Can not run CAN FD ( S32K 146-Q144(S32K146EVB))

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not run CAN FD ( S32K 146-Q144(S32K146EVB))

Jump to solution
815 Views
Palawut
Contributor I

Hi 
I have a few question about S32K 146

this board : S32K146-Q144 (S32K146EVB) suppose to support CAN FD but 
its transceivers ( TJA1027) do not support CAN FD (SUPPORT ONLY LIN)
I have to work currently with CAN FD. What Should i do? can you suggest me 
1. If i need to add new transceiver ( that can support CAN FD) which one you recommend

2. If i want to buy a new main board and stuff to work with CAN FD functionally what do you suggest?

0 Kudos
Reply
1 Solution
797 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The CAN signal is connect to the UJA1169TK/F on S32K146EVB(not connect to TJA1027).

UJA1169TKF S32K146EVB.png

Please read the file:///C:/NXP/S32DS.3.4/S32DS/software/S32SDK_S32K1XX_RTM_4.0.2/doc/html_S32K146/can_pal_s32k146_group.htmlCAN PAL.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
798 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The CAN signal is connect to the UJA1169TK/F on S32K146EVB(not connect to TJA1027).

UJA1169TKF S32K146EVB.png

Please read the file:///C:/NXP/S32DS.3.4/S32DS/software/S32SDK_S32K1XX_RTM_4.0.2/doc/html_S32K146/can_pal_s32k146_group.htmlCAN PAL.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
784 Views
Palawut
Contributor I

which means the UJA1169TK/F on S32K146EVB can also run CAN FD normally without adding anything ?
https://www.nxp.com/products/power-management/pmics-and-sbcs/mini-sbcs/mini-high-speed-can-system-ba...

 

i need you to confirm what i just understand 
Thank you for your answer 

0 Kudos
Reply