Can not debug S32K144EVB with PEMicro multilink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can not debug S32K144EVB with PEMicro multilink

1,735件の閲覧回数
lwcall2007
Contributor I

I use S32K144EVB to study S32K144 , i can debug S32K144 with OpenSDA , but fail to debug it with my PEMicro multilink device

0 件の賞賛
3 返答(返信)

1,700件の閲覧回数
JustVb
Contributor III

I met the same problem,maybe there is something wrong with your debugger hardware.

I used another debugger, the problem was solved.

0 件の賞賛

1,723件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi lwcall2007,

Please notice the 1st pin of SWD CONNECTOR(J14), red line should be connect at 1st pin.

SWD CONNECTOR J14.jpg

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛

1,715件の閲覧回数
lwcall2007
Contributor I

I have tried to exchange the SWD pin connection , but it still does not work

0 件の賞賛