Dear sir,
I am using the S32K116 sample and convert the 4 channel ADC0 by PDB back-to-back mode. From ADC0_CH3 to ADC0_CH6.
I want to use compare value function only in ADC0_CH4 & ADC0_CH5.
Can I set the Compare Value function for ADC0_CH4 & ADC0_CH5 iADC interruptn an before the ADC0_CH4 conversion and unset the compare Value function after the ADC0_CH5 conversion?
( for example : set ADC0->CV[0] ,ADC0->CV[1], ADC_SC2_ACFE(x), ADC_SC2_ACFGT(x), ADC_SC2_ACREN(x) )
If not, could you give me some suggestions to realize this requirement?
Thanks & BRs,
XIECLOCK
ADC_handle
PDB_init
Solved! Go to Solution.
Hello Jerry,
The CS2 register cannot be modified while there is a conversion in progress, the conversion would be aborted.
So, it is not possible in the PDB back-to-back mode.
But you can use PDB with a separate delay for each channel instead of the back-to-back mode.
And change the CS2 register within a delay.
Best regards,
Daniel
Hello Jerry,
The CS2 register cannot be modified while there is a conversion in progress, the conversion would be aborted.
So, it is not possible in the PDB back-to-back mode.
But you can use PDB with a separate delay for each channel instead of the back-to-back mode.
And change the CS2 register within a delay.
Best regards,
Daniel