Can I get a software base project of S32k144 with IAR IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I get a software base project of S32k144 with IAR IDE

608 Views
DELPHI_Eric
Contributor III

Can I get a software base project of S32k144 with IAR IDE,thanks.

0 Kudos
1 Reply

518 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi shen jun

There is a plug in with S32 Design Studio IDE which you can create a project for IAR base. Please check the following poast:

HOWTO: Export S32DS Project to IAR EW (S32K14x/S32K11x) 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos