CSEc Keys and User Data on the 4kB EERAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSEc Keys and User Data on the 4kB EERAM

Jump to solution
1,136 Views
nevozade
Contributor IV

Hello, 

I am working on S32K148 and I am going to enable CSE module for secure booting. According to the application note ('Using S32K148 FlexNVM Memory', AN12003, Rev.0, July 2017), in section 3.3, 64 kB of the FlexNVM are used as E-flash (EEPROM backup and key storage together) and CSEc uses up to 512 Bytes for key storage, leaving EEPROM to use the remaining 3.5 kB EERAM for the EEPROM and CSEc enabled use case (attached). 

What I'm wondering about in this usage is whether the user data is somehow preserved overwriting or deleting the registered keys. Briefly, I want to know whether the 512 bytes where the keys are recorded are randomly recorded in this EERAM or are they recorded in specific locations such as the beginning/end of the 4 kB FlexRAM.

I urge you to assist in this matter.

Best Regards.

0 Kudos
Reply
1 Solution
1,124 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @nevozade,

If the allocated CSEc space is 512B, the space 0x14000E00-0x14000FFF will not be accessible in the FlexRAM (EEPROM).

Any access to this region generates a bus fault exception.

 

Regads,

Daniel

 

View solution in original post

0 Kudos
Reply
1 Reply
1,125 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @nevozade,

If the allocated CSEc space is 512B, the space 0x14000E00-0x14000FFF will not be accessible in the FlexRAM (EEPROM).

Any access to this region generates a bus fault exception.

 

Regads,

Daniel

 

0 Kudos
Reply