Where is S32K1xx_DMA_INT_mapping.xlsm?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is S32K1xx_DMA_INT_mapping.xlsm?

1,091 Views
filu
Contributor I

filu_0-1641868851529.png

 


The file 'S32K1xx_DMA_INT_mapping.xlsm' written on p.117 of 'S32K1xx Series Reference Manual Rev. 14' (S32K-RM.pdf) does not appear in the attachment.

 

https://community.nxp.com/t5/S32K/where-to-get-the-file-quot-S32K1xx-DMA-INT-mapping-xlsm-quot/m-p/7...

https://community.nxp.com/t5/S32K/about-S32K1xx-DMA-INT-mapping-xlsm/m-p/676527

From this post, it looks like it is attached to the old version, but where can I download the old reference manual?

0 Kudos
4 Replies

1,086 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi filu,

I will send you the Rev. 13 S32K-RM. Let me check what's wrong with the latest Rev. 14' S32K1xx Series Reference Manual Rev. 14.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,023 Views
mks004
Contributor II

I am running into the same issue. Where can one find S32K1xx_DMA_INT_mapping.xlsm?

0 Kudos

989 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi @junxi_cai @mks004,

Sorry for the inconvenience we bring you!
Please keep using the S32K1xx_DMA_INT_mapping in Rev13 until the documentation department fixes this issue.

Best Regards,
Robin

0 Kudos

1,054 Views
junxi_cai
Contributor II

Hello Robin,

I have the same issue, could you please also share the S32K-RM REV.13 with me?

Thank you,

Junxi 

0 Kudos