Hello,
Are the MISO and MOSI pins labeled incorrectly in the CANHUBK344 Eval Board Schematic?
Thank you!
Vusal
Solved! Go to Solution.
Hi Vusal,
Please read the 70.6.1.9 Configuration 1 (CFGR1) of S32K3XXRM Rev8.
25-24 PINCFG Pin Configuration
Specifies the pins used for input and output data during serial transfers. This field is ignored when performing parallel transfers.
00b - SIN is used for input data; SOUT is used for output data
01b - SIN is used for both input and output data; only half-duplex serial transfers are supported
10b - SOUT is used for both input and output data; only half-duplex serial transfers are supported
11b - SOUT is used for input data; SIN is used for output data
Since the LPSPI of S32K3 has this function, it is OK to label the MISO and MOSI pins in this way.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Vusal,
Please read the 70.6.1.9 Configuration 1 (CFGR1) of S32K3XXRM Rev8.
25-24 PINCFG Pin Configuration
Specifies the pins used for input and output data during serial transfers. This field is ignored when performing parallel transfers.
00b - SIN is used for input data; SOUT is used for output data
01b - SIN is used for both input and output data; only half-duplex serial transfers are supported
10b - SOUT is used for both input and output data; only half-duplex serial transfers are supported
11b - SOUT is used for input data; SIN is used for output data
Since the LPSPI of S32K3 has this function, it is OK to label the MISO and MOSI pins in this way.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Robin,
Thank you for pointing this out! It makes sense in that case.
Best,
Vusal