CANHUBK344 Eval Board LPSPI1 MISO and MOSI pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CANHUBK344 Eval Board LPSPI1 MISO and MOSI pins

ソリューションへジャンプ
211件の閲覧回数
vusal
Contributor III

Hello,

Are the MISO and MOSI pins labeled incorrectly in the CANHUBK344 Eval Board Schematic?

vusal_0-1719530700887.png


Thank you!

Vusal

 

0 件の賞賛
返信
1 解決策
198件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Vusal,

Please read the 70.6.1.9 Configuration 1 (CFGR1) of S32K3XXRM Rev8.

25-24 PINCFG     Pin Configuration
Specifies the pins used for input and output data during serial transfers. This field is ignored when performing parallel transfers.
00b - SIN is used for input data; SOUT is used for output data
01b - SIN is used for both input and output data; only half-duplex serial transfers are supported
10b - SOUT is used for both input and output data; only half-duplex serial transfers are supported
11b - SOUT is used for input data; SIN is used for output data

Since the LPSPI of S32K3 has this function, it is OK to label the MISO and MOSI pins in this way.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
199件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Vusal,

Please read the 70.6.1.9 Configuration 1 (CFGR1) of S32K3XXRM Rev8.

25-24 PINCFG     Pin Configuration
Specifies the pins used for input and output data during serial transfers. This field is ignored when performing parallel transfers.
00b - SIN is used for input data; SOUT is used for output data
01b - SIN is used for both input and output data; only half-duplex serial transfers are supported
10b - SOUT is used for both input and output data; only half-duplex serial transfers are supported
11b - SOUT is used for input data; SIN is used for output data

Since the LPSPI of S32K3 has this function, it is OK to label the MISO and MOSI pins in this way.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

185件の閲覧回数
vusal
Contributor III

Hi Robin,

Thank you for pointing this out! It makes sense in that case.

Best,

Vusal

0 件の賞賛
返信