When I configure the can mailbox of S32K144, should I configure this register to configure the maximum number of mailboxes of S32K144?
CAN0->MCR = 0x0000000F | CAN_MCR_SRXDIS(1); /* Negate FlexCAN 1 halt state for 32 MBs */
After the configuration is complete, the can IFLAG register is checked and the received data is stored in only one mailbox. All the other mailboxes are empty
Hi leonordo,
Please refer to the examples in the article: S32K1xx SDK FlexCAN sample projects to demonstrate its basic and advanced features
Best Regards,
Robin
Hello, I have solved the problem before, because I did not initialize the mailbox configuration;
Now I have another question: Can S32K144 email address not be configured as:
Three mailboxes receive the same ID at the same time, mailbox one is full, mailbox two is receiving, and so on until all three mailboxes are full