I develope ECU related CAN FD.
CAN sample point is not set as below in processor expert.
<Setting parameter of processor expert>
1) Enable FD : Yes
2) PE clock source : Sys clock
3) Operation Mode : Normal mode
4) Payload Size : 16
5) Module clodk : 80Mhz
6) PE clock : 80Mhz
* Arbitraion phase *
- Propagation segment : 47
- Phase segment 1 : 14
- Phase segment 2 : 15
- Prescaler Division Factor : 1
- Resync jump width : 16
Qes) By S32K144 Reference Manual(page 1659), Arbitration phase condition of CAN FD
(using CAN_CBT) is as below. Why my setting(Phase segment 1, Phase segment 2, Resync jump width)
can not be generated code in processor expert ?
1) Condition of Time Segment 1 : 2 <= x <= 96
-> My setting : Propagation segment(47) + Phase segment 1(14) + 2, all sum is 63, condition(2<= x <=96) is meet
2) Condition of Time Segment 1 : 2 <= x <= 32
-> My setting : Phase segment 2(15) + 1, all sum is 16, condition(2<= x <= 32) is meet
Remark) My target Arbitration of CAN FD setting is as below
1) Target CAN speed : 500k bps
2) PE Clock : 80MHz
3) Baud rate prescaler : 2
4) TQ : 80 TQ
5) TSEG1 : 63 TQ
6) TSEG2 : 16 TQ
7) Sample point : 80%
8) SJW : 16
Thank you.
Hi,
Seems the PE’s FlexCAN component checks the given values against CTRL1 register even if the FD is enabled and CBT should be used.
You can use below functions in your code to set desired bitrate for both the arbitration and data phase:
FLEXCAN_HAL_SetTimeSegments(base, &bitrate); // set arbitration bitrate
FLEXCAN_HAL_SetTimeSegmentsCbt(base, &bitrate); // set data bitrate
BR, Petr
Hi Petr
Thank you for your response.
Still CAN bit rate values can not be modified in processor expert.
So I change generated code(canCom1.c file) as below. And then working well without Error frame.
But I hope that can modify this point in processor expert. Because below code is return to generated code
when generating code in processor expert.
flexcan_user_config_t canCom1_InitConfig0 = {
...
.bitrate = {
#if 0
.propSeg = 7,
.phaseSeg1 = 6,
.phaseSeg2 = 3,
.preDivider = 7,
.rJumpwidth = 1
#endif
/* for Extended bit rate for CAN FD */
#if 1
.propSeg = 47,
.phaseSeg1 = 14,
.phaseSeg2 = 15,
.preDivider = 1,
.rJumpwidth = 16
#endif
}
...
};
Hi Jaewoo,
You should not modify modules generated by PE. Your changes can be rewritten back by PE once code is generated again.
That’s why it is advisable to use above mentioned functions.
Or if “canCom1_InitConfig0” structure is not defined as const (read only options deselected in the component setting) then you can modify “bitrate” parameters before FLEXCAN_DRV_Init() is called.
BR, Petr