在CAN中断中;
CAN配置为const flexcan_user_config_t canCom1_InitConfig1 = {
.fd_enable = false,//启用/禁用灵活数据速率功能
.pe_clock = FLEXCAN_CLK_SOURCE_SOSCDIV2,//CAN时钟源
.max_num_mb = 16,//消息缓冲区的最大数目
.num_id_filters = FLEXCAN_RX_FIFO_ID_FILTERS_8,//需要的RX FIFO ID过滤器的数目
.is_rx_fifo_needed = false,//1启用; 0停用。这可以控制Rx FIFO功能是否启用
.flexcanMode = FLEXCAN_NORMAL_MODE,//用户可配置的FlexCAN操作模式, FLEXCAN_NORMAL_MODE;正常模式或用户模式;FLEXCAN_LISTEN_ONLY_MODE:只听模式;
//FLEXCAN_LOOPBACK_MODE: 环回模式; FLEXCAN_FREEZE_MODE睡眠)冻结模式;FLEXCAN_DISABLE_MODE 模块禁用模式
.payload = FLEXCAN_PAYLOAD_SIZE_8,//指定的邮箱的有效载荷字节大小
.bitrate = { //用于标准帧的比特率或FD帧的仲裁阶段
.propSeg = 7,//传播段
.phaseSeg1 = 4,//相位段1
.phaseSeg2 = 1,//相位段2
.preDivider = 0,//时钟分频器分因子
.rJumpwidth = 1 //同步跳转宽度
},
.bitrate_cbt = { //用于FD帧的数据阶段的比特率
.propSeg = 7,//传播段
.phaseSeg1 = 4,//相位段1
.phaseSeg2 = 1,//相位段2
.preDivider = 0,//时钟分频器分因子
.rJumpwidth = 1//同步跳转宽度
},
采用16通道接收, FLEXCAN_DRV_ConfigRxMb(0,16, &dataInfo, 0x1800FCF4);//配置接收FlexCAN0(Rx)消息缓冲区
中断配置为: INT_SYS_EnableIRQ(CAN0_ORed_16_31_MB_IRQn);//为给定的IRQ号码启用中断。
INT_SYS_SetPriority(CAN0_ORed_16_31_MB_IRQn,0U);//设置中断优先级。
采用17通道发送:FLEXCAN_DRV_ConfigTxMb(0,17,&tx_info,0x12);//FlexCAN发送消息缓冲区配置。
FLEXCAN_DRV_Send(0U,17U,&tx_info,0x18f0000f,mb_data );//FlexCAN0发送消息
为什么接收没有进入void CAN0_ORed_16_31_MB_IRQHandler(void)
{
FLEXCAN_IRQHandler(0U);
}
发送却时进入了:void CAN0_ORed_16_31_MB_IRQHandler(void)
{
FLEXCAN_IRQHandler(0U);
}
Hi,
seems you enable only first 16 message buffers (MB0-MB15), but use MB16 and MB17 for RX and TX operation.
This will not work. What is the status driver functions return?
Try to use MB with number between 0-15 or increase anount of MB used for communication, defined by "max_num_mb".
BR, Petr
hello,
A issue is reproduced. Would share the mitigation how to fix the issue, thank you.