About the sliding factors of the LPO frequency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the sliding factors of the LPO frequency

Jump to solution
658 Views
Hozumi
Contributor I

The S32K1xx LPO frequency has the following specifications:
Min. 113kHz, Typ. 128kHz, Max 139 kHz

What is the LPO frequency sliding factor?
temperature? Or is it a manufacturing issue?
Can NXP provide the probability of working with Typical?

0 Kudos
1 Solution
643 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Hozumi,

It depends on the temperature and it differs part-to-part from the manufacturing too.

The LPO is trimmed as close to 128KHz as possible in the production.

danielmartynek_0-1661781606922.png

For example, LPOTRIM can be pre-programmed to 0x1D in the production.

One LPOTRIM step gives about 3kHz difference in the LPO frequency.

Measured default frequency 129kHz (CLKOUT).

Trimmed to 0x1C (one step up) = 132kHz

Trimmed to 0x1E (one step down) = 126kHz

That means that just from the production, the LPO can be 128KHz +- 1.5kHz.

 

Regards,

Daniel

 

 

 

 

 

 

 

 

 

 

View solution in original post

0 Kudos
3 Replies
644 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Hozumi,

It depends on the temperature and it differs part-to-part from the manufacturing too.

The LPO is trimmed as close to 128KHz as possible in the production.

danielmartynek_0-1661781606922.png

For example, LPOTRIM can be pre-programmed to 0x1D in the production.

One LPOTRIM step gives about 3kHz difference in the LPO frequency.

Measured default frequency 129kHz (CLKOUT).

Trimmed to 0x1C (one step up) = 132kHz

Trimmed to 0x1E (one step down) = 126kHz

That means that just from the production, the LPO can be 128KHz +- 1.5kHz.

 

Regards,

Daniel

 

 

 

 

 

 

 

 

 

 

0 Kudos
640 Views
Hozumi
Contributor I

Thank you for your prompt reply.

Just to make sure, is the trimming done by the NXP side before shipping?

And one more question, Is it possible for the LPO frequency to fluctuate during operation?

0 Kudos
632 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Hozumi,

Yes, it is trimmed by NXP.

The frequency depends on the operational conditions like temperature, but the dependency is not specified.

 

BR, Daniel

0 Kudos