About S32K144 Flash Write Read Erase

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About S32K144 Flash Write Read Erase

969件の閲覧回数
alexwu
Contributor I

Dear,

Can you supply code sample about "FLASH write / erase / read" based on S32K144 core chipset.

Thanks.

Alex

0 件の賞賛
2 返答(返信)

800件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Alex Wu

The Flash_partitioning example project that comes with the S32DS (using the SDK) makes those operations as a part of the example code, you can check it and please tell us if you have any question about it.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you
-------------------------------------------------------------------------------

0 件の賞賛

800件の閲覧回数
alexwu
Contributor I

Dear TIC,

What I want to do is to open EEE area to use it as power loss data storage.

But as I understood, If partition the FLASH, all my data includes code data will be lost, Right?

I hope you have EEE code sample for reference.

--

Thanks.

Alex

0 件の賞賛