AIPS_ PLAT_ CLK and AIPS_ SLOW_ CLK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

AIPS_ PLAT_ CLK and AIPS_ SLOW_ CLK

跳至解决方案
481 次查看
shiqi_seventeen
Contributor III

Hello Team

I am using S32K312,there are some questions abou CLOCK.

I have a few questions :

1. AIPS_ PLAT_ CLK and AIPS_ SLOW_ CLK ,What does  mean about them?

2. AIPS_ PLAT_ CLK and AIPS_ SLOW_ CLK  ,What is the difference or connection between them?

3. AIPS_ PLAT_ CLK and AIPS_ SLOW_ CLK, What peripherals are CLK used on, or how should I choose them as the clock source for peripherals?

Thanks

0 项奖励
回复
1 解答
467 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please download S32K3xx MCU Family - Reference Manual and read the 24.6 Peripheral clocking and 24.3.8 S32K312 clock system diagram.

24.6 Peripheral clocking.png

AIPS_PLAT_CLK (medium-speed peripheral clock) (MC_CGM.MUX_0_DC_1[DIV])
AIPS_SLOW_CLK (slow-speed peripheral clock) (MC_CGM.MUX_0_DC_2[DIV])

24.3.8 S32K312 clock system diagram.png

If you are using S32DS, S32 Configuration Tool may help you understand it better.

S32CT Clocks tool S32K312.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
468 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please download S32K3xx MCU Family - Reference Manual and read the 24.6 Peripheral clocking and 24.3.8 S32K312 clock system diagram.

24.6 Peripheral clocking.png

AIPS_PLAT_CLK (medium-speed peripheral clock) (MC_CGM.MUX_0_DC_1[DIV])
AIPS_SLOW_CLK (slow-speed peripheral clock) (MC_CGM.MUX_0_DC_2[DIV])

24.3.8 S32K312 clock system diagram.png

If you are using S32DS, S32 Configuration Tool may help you understand it better.

S32CT Clocks tool S32K312.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复