A problem occur when I import  a example from S32_SDK_S32K1xx_RTM_4.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A problem occur when I import  a example from S32_SDK_S32K1xx_RTM_4.0.0

1,102 Views
wzslaoman
Contributor I

 I can't find a symbol "ATTACHED_SDK_VERSION" in project settings.

IDE VERSION: S32 Design Studio for ARM 2.2

pastedImage_2.png

pastedImage_1.png

Tags (1)
0 Kudos
Reply
5 Replies

1,019 Views
suchunlee
Contributor I

I can't find a symbol "ATTACHED_SDK_VERSION" in project settings.

IDE VERSION: S32 Design Studio for ARM 3.3             SDK:S32_SDK_S32K1xx_RTM_4.0.0    

微信截图_20201028152236.png

 

 

0 Kudos
Reply

1,043 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Mark,

After download and install the S32_SDK_S32K1xx_RTM_4.0.0, I was able to see the S32SDK_for_S32K1xx_RTM_4.0.0_ReleaseNotes in folder (C:\NXP\S32_SDK_S32K1xx_RTM_4.0.0).

S32SDK_for_S32K1xx_RTM_4.0.0_ReleaseNotes.png

The "6.3 Compiler and IDE versions" shows that the S32 Design Studio 3.3 IDE support S32_SDK_S32K1xx_RTM_4.0.0. 

Moving forward the support for S32K1xx / S32K1xxW will be integrated as part of the S32 Design Studio for S32 Platform. You can find the latest version (v3.3 released June 2020), in the Downloads tab of this IDE variant:

S32 Design Studio | NXP 

S32 Design Studio 3.3.png

Unfortunately:

There are still some errors when build the project of SDK4.0.0 using S32DS 3.3. 
"By default, There was no platform integrated in S32DS. In order to use S32DS for S32K1xx. Users need to install the development package for S32K1xx but this package is from another team We are in discussion with that team to request them publish it"

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,043 Views
wzslaoman
Contributor I

Thank you for your reply,I hope it will support earlier.

0 Kudos
Reply

1,043 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Mark,

All updates for RTM 4.0.0 are available in Design Studio as update sited. Please check and let us know if you have other issues.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,019 Views
suchunlee
Contributor I

I can't find a symbol "ATTACHED_SDK_VERSION" in project settings.

IDE VERSION: S32 Design Studio for ARM 3.3             SDK:S32_SDK_S32K1xx_RTM_4.0.0    

 

微信截图_20201028152236.png

 

0 Kudos
Reply