A Bug of S32DS and SDK(FreeRTOS 1.0.0.202108310250)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A Bug of S32DS and SDK(FreeRTOS 1.0.0.202108310250)

Jump to solution
1,705 Views
JustVb
Contributor III

I use Configuration Tools to config osif module and set "Operation System Type" as FreeRTOS and and OS module. 

Then the Macro "USING_OS_FREERTOS" was defined both  in the generated code "OsIf_Cfg.h" and in build tool settings, which led to complie warning

JustVb_3-1639808019539.png

JustVb_1-1639807854217.png

JustVb_0-1639807741160.png

 

JustVb_2-1639807865024.png

 

 

Tags (1)
0 Kudos
1 Solution
1,551 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @JustVb,

I've got your situation. Let me discuss with the team to find out the appropriate way to integrate. Thanks for your report.

Best Regards,

Nam

View solution in original post

0 Kudos
9 Replies
1,624 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @JustVb,

It's a good video, however please share me your project (FreeRTOS_test), so that I can import to my S32DS and test it. It would be easier for me than looking into the video. You just need to archive the project and share via here.

Best Regards,

Nam

0 Kudos
1,610 Views
JustVb
Contributor III

helle,namnguyenviet,

here is the test project.I wish you would replay it, thanks.

Best Regards.

0 Kudos
1,587 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @JustVb,

I have removed all of the redundant symbol in "Path and Setting". Basically, I just click to "Remove" button and then "Apply". I have attached the project after fixed.

Best Regards,

Nam

0 Kudos
1,568 Views
JustVb
Contributor III

hello, namnguyenviet:

  did you try to use the "configuration tools" to re-generate code?

when I regenerated code, the macro definition came back again.

0 Kudos
1,552 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @JustVb,

I've got your situation. Let me discuss with the team to find out the appropriate way to integrate. Thanks for your report.

Best Regards,

Nam

0 Kudos
1,653 Views
namnguyenviet
NXP Employee
NXP Employee

In that case, please share me the project. I will double check in my site.

Best Regards,

Nam

0 Kudos
1,645 Views
JustVb
Contributor III

Thanks for your reply, the attachment is the screen record of the operation details.

Best Regards!

0 Kudos
1,668 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

Then you need to remove the definition in the "Path and symbol" setting. Normally it shall be modified by users.

Best Regards,

Nam

0 Kudos
1,662 Views
JustVb
Contributor III

II removed the definition in the "Path and symbol" setting,but the configuration tools will add it back when I generate code again

0 Kudos