s32g2 firmware developper required

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32g2 firmware developper required

888件の閲覧回数
ilir
Contributor I

hi all admin delete if not allowed

i have hired someone to build me a pcb with s32g2 cpu but i need someone to build me the firmware is there someone who could do it thank all 

0 件の賞賛
返信
3 返答(返信)

884件の閲覧回数
ilir
Contributor I

max485 or AU5780 for j1850 vpw
XG7100 for j1850 pwm
TJA1024 lin transreciver
MC33660BEF k line
TJA1083G flexray
can-canfd TJA1462AT
cortex bdm jtag module 5 ports
ATWINC3400-MR210CA131 wifi/bluetooth
usb type c 3.1
usb 2.0 3.0
ethernet port TJA1101

those are the options for now 

0 件の賞賛
返信

851件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

842件の閲覧回数
ilir
Contributor I

hi thx for the reply

even if i buy it i cant make the firmware i need a developper to do it thats why iam not a firmware developper actually iam looking to hire someone to do it 

0 件の賞賛
返信